{}

我们的品牌

欢迎访问施耐德电气网站

欢迎访问我们的网站。
搜索常见问题解答
在一个Unity项目中可以配置多少BMENOC0321?
问题描述:
Unity pro 编程的项目中可以配置BMENOC0321的最大数量。

所属产品线:
过程自动化控制平台

解决方法:

M580系统的本地机架最多可以使用2个BMENOC0321模块,提供控制网络和现场设备之间的以太网透明性。
注意:如果两个BMENOC0321在同一个机架上,可能只有一个IP可以启用。
注意:BMENOC0321也可以在M580热备份系统中使用。M580热备份使用两个物理模块。一个在主机架,另一个在备用机架。



是否有帮助?

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.