我们的品牌

欢迎访问施耐德电气网站

欢迎访问我们的网站。

Overview

Schneider Electric’s control network interface (CNI) is an industrialized, high-availability, embedded method for interconnecting multiple EcoStruxure Foxboro DCS to provide greater operational efficiency and effectiveness. The CNI can also partition an EcoStruxure Foxboro DCS into independent but linked, stand-alone systems to protect operational integrity.

Features

  • Ability to upgrade selected areas without impacting entire system
  • Ability to isolate sections for reduced risk of cybersecurity vulnerability
  • Ability to efficiently adapt operations and achieve compliance
  • Fast, accurate view of production data across the plant
  • Better, more informed decision-making to optimize plant production
  • Easy sharing of operational data across geographically dispersed systems for maximized efficiency

Benefits

  • Operate multiple EcoStruxure Foxboro DCS “as one system”
  • Minimize system maintenance and engineering efforts
  • Expand and adapt with minimum impact on operations
  • Provide greater situational awareness and faster response times
  • Protect business-sensitive data to retain competitive advantage
  • Isolate operations to reduce risk of downtime

Applications

  • Refining and petrochemicals
  • Upstream and midstream oil and gas
  • Chemicals and specialty chemicals
  • Power generation
  • Metals, mining and minerals
  • Water and wastewater
  • Food and beverage
  • Life sciences and pharmaceuticals

需要帮助?

从此处开始!

立即找到答案。自行搜索解决方案,或者联系我们的专家。

获取支持

我们的客户关爱团队可为您提供详细信息、技术支持、投诉帮助等服务,请联系他们。

浏览常见问题解答

通过浏览与主题相关的常见问题解答 (FAQ),获取您需要的答案。

 opens in new Window

我要采购

开始在线采购咨询,专家将会与您联系!

 opens in new Window

Chat

您是否有问题需要我们协助?